Goals and Symptoms
Does the unit produce significant amount of harmonics that could damage output wiring on startup.
Facts and Changes
Difference with shorting contactor and without shorting contactor wiring is burning up over period of time and they thought this may be an issue
Causes and Fixes
The harmonics level at the output of ATS is very low and only during the acceleration. May be the problem come from the section of your wire or the tightening.
Legacy KB System (APS) Data: RESL157597 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altistart 46
發佈於:施耐德電機Taiwan