Issue
How do I read or write a program to/from the SY/MAX model 50 controller's memory pack to the 8005PR4 hand held programmer's PROM burner socket?
Product Line
SY/MAX
Environment
8005PR4
Resolution
First ensure you have the memory pack installed in the 8005PR4's PROM burner socket.
To read a program from the SY/MAX model 50 controller's memory pack to the 8005PR4 enter the following sequence:
- PROM, READ.
- Once "PROM READ GO?" is displayed press the ENTR key. "PROM READ" is displayed during execution.
- When completed "PROM READ END" is displayed.
To write a program from the 8005PR4 to the SY/MAX model 50 controller's memory pack enter the following sequence:
- PROM ENTR.
- Once "PROM WRIT GO?" is displayed press the ENTR key. "PROM WRIT" is displayed during execution.
- When completed "PROM WRIT END" is displayed.
發佈於:施耐德電機Taiwan