Issue
What is the difference between a Standard SY/MAX model 300 controller and a Deluxe model 300 SY/MAX controller?
Product Line
SY/MAX
Environment
8020SCP311
Resolution
A Standard SY/MAX model 300 controller performs relay ladder diagram logic, counting and timing functions. It can also perform BCD to Binary and Binary to BCD conversions, Master control relay, Synchronous shift registers and Immediate I/O update.
Deluxe SY/MAX model 300 controllers perform all the functions of a standard model and additionally offer Asynchronous shift registers, Add, subtract, Multiply Divide, Print and communications functions.
發佈於:施耐德電機Taiwan