{}
搜尋常見問題
What is the difference between the 8020SCP423 and 8020SCP424 SY/MAX controllers?

Issue

What is the difference between the 8020SCP423 and 8020SCP424 SY/MAX controllers?

Product Line

SY/MAX

Environment

8020SCP423

Resolution

The only difference between the 8020SCP423 and 8020SCP424 SY/MAX controllers is the size of their user memory. The 8020SCP423 has 8K of RAM. The 8020SCP424 has 16K of RAM.

施耐德電機Taiwan