Issue
Is there any way to display used references in a Modsoft program while OFF-LINE from the controller?
Product line
Modsoft
Environment
Modsoft
Resolution
No. Modsoft can display used references in a PLC program only while ON-LINE with a controller. Modsoft can also print out used references as part of printing a program, but cannot dispaly them while OFF-LINE from a controller. To display the Used References while on-line with a controller, first go open any ladder logic network ,then select "Refs" from the top tool-bar. The "Used References" option will appear in that pull-down menu.
發佈於:施耐德電機Taiwan