The following fuse part numbers are used in the Telefast 2 PreWired System Connection Interfaces:
Fuse Rating | Part Number |
0.125 A | ABE7FU012 |
0.5 A | ABE7FU050 |
1 A | ABE7FU100 |
2 A | ABE7FU200 |
4 A | ABE7FU400 |
6.3 A | ABE7FU630 |
These fuses are fast blow, 5 x 20mm, 250V and have a quantity of 10 per package.
發佈於:施耐德電機Taiwan