{}

我們的品牌

Impact-Company-Logo-English Black-01-177x54

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
搜尋常見問題
What is the cable part number to connect a Quantum with a 9 pin Sub-D serial port to a TSXCUSB232?
Issue:
Cable part number to connect a Quantum with a 9 pin Sub-D serial port to a TSXCUSB232


Product Line:
Quantum PLC


Resolution:

The Quantum DB9 RS-232 programming cable for that adapter is available in two lengths:
990NAA26320.....12 feet (3.66 meters)
990NAA26350.....50 feet (15.24 meters)

施耐德電機Taiwan

探索更多
系列:
可能有幫助的文章
探索更多
系列: