Issue
The purpose of this resolution is to document the 984 Chassis Mount AM-C921-100 Communications Processor port pinouts.
Product Line
AM-C921
Resolution
(Removed File URL: 187468_20E6/C921-101.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/7f37013e71000763c125733200160dc1/fl_block_5/0.54E?OpenElement&FieldElemFormat=gif) (Removed File URL: 187468_20E6/C921_Ports.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/7f37013e71000763c125733200160dc1/fl_block_5/0.1038?OpenElement&FieldElemFormat=gif)
Legacy KB System (APS) Data: RESL187468 V1.0, Originally authored by WeDa on 08/09/2007, Last Edited by WeDa on 08/09/2007
Related ranges: Modicon 1/2/3/4/5/8/984s
發佈於:施耐德電機Taiwan