Issue
The purpose of this resolution is to inform users of the Advantys STBART0200 Thermocouple/RTD module that the ranges for the J, R, & S thermocouples have been expanded to match the ranges in other Schneider offerings.
Product Line
Advantys STB
STBART0200
Environment
Resolution
STBART0200 modules with an SV 1.60 and higher have the expanded thermocouple ranges. The STBART0200 modules cannot be field upgraded.
The new ranges have been updated in the Advantys STB Analog I/O Modules Reference Guide dated 4/2007 and are as follows:
發佈於: 施耐德電機Taiwan