{}
搜尋常見問題
What is the pinout to the RS485 cable needed to connect an M340 to a Unity Quantum RJ45 modbus port?

Note: If the cable is 10 feet or longer a 120 ohm resistor will be needed across pins 1 and 2 on the Quantum side as well as pins 4 and 5 on the M340 side.


施耐德電機Taiwan

探索更多
系列:
可能有幫助的文章
探索更多
系列: