搜尋常見問題
Illumination power and service life for XVBL0M5 .
Goals and Symptoms
Illumination power and service life for XVBL0M5 .
Facts and Changes
XVBL0M5
Causes and Fixes
The life time is 100 000 hours without maintenance (11 years continuous operation).
The values given are an average for all colors.
230 cd/m² without light diffuser.
With light diffuser 140 cd/m²
Legacy KB System (APS) Data: RESL197903 V1.0, Originally authored by LaBe on 02/27/2009, Last Edited by LaBe on 02/27/2009
Related ranges: Harmony XVB
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: