Issue
The purpose of this resolution is to inform Momentum M1E users that the 984LL firmware has been upgraded (Aug. 2009) to version 1.30.
Product Line
Momentum
171CCC96020 Processor
171CCC98020 Processor
171CCC96030 Processor
171CCC98030 Processor
Environment
Resolution
984LL firmware version 1.30 contains the following enhancement:
A configurable TCP/IP retransmission timer for the MSTR function block.
- This enhancement is not supported in the Concept MSTR DX Zoom screens at this time.
- Resource file MSTR.URF for ProWORX NxT and resource file MSTR.UCS for ProWORX32 are included.
A description of the new MSTR function is explained in the attachment Resolution document.
The attached zip file contains the following files:
m1ev130.bin M1E firmware
m1 v130 Resolution.doc Resolution
MSTR.ucs ProWORX32 resource file
MSTR urf ProWORX NxT resource file
發佈於: 施耐德電機Taiwan