搜尋常見問題
Cannot download to the STBNIP221 after updating to version 2.71
Issue
Cannot download to theSTBNIP221 after updating to version 2.71
Product Line
STBNIP2212
Environment
Windows 7
Resolution
This could happen if the application was created in an older version of the Advantys Configuration Software
and that same version is being used to perform the download.
To resolve the problem:
- Update to the latest version of the Advantys Configuration Software.
- Open the project.
- Click on 'File\Save' to save the project.
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: