Issue
Replacement part number
Product Line
Magelis
Resolution
The recommended replacement is the Magelis HMIGK2310 HMI. The software needed to program this terminal is Vijeo Designer. The application in the XBTF011110 is not compatible with the HMIGKxxxx terminals. You would need to recreate the application in Vijeo Designer.
發佈於: 施耐德電機Taiwan