搜尋常見問題
What cables are available to be used with the BMXDDI1602 or the BMXDDO1602 ?
There is one type of cable, available in three lengths.
One 20-way terminal block on one end and flying leads on the other end.
BMXFTW301 - 3 meter
BMXFTW501 - 5 meter
BMXFTW1001 - 10 meter
Related ranges: Modicon M340
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: