One possible cause is that the PLC is using a PCMCIA card in slot 1 that has a bad battery. A bad battery is indicated by PCM1 with the number flashing on the LCD display. In PLC logic, %S67 (PCMCIABAT0) can be monitored.
發佈於:施耐德電機Taiwan


{}
One possible cause is that the PLC is using a PCMCIA card in slot 1 that has a bad battery. A bad battery is indicated by PCM1 with the number flashing on the LCD display. In PLC logic, %S67 (PCMCIABAT0) can be monitored.