搜尋常見問題
What are the screw size and wire size for the CT and PT terminal connections on the PM820 and PM850 meters?
Issue:
A user requires the information of the screw size and wire size, for the CT and PT terminal connections on the PM820 and PM850 meters.
Product Line:
PM800 series meters
Cause:
A user requires the information of the screw size and wire size, for the CT and PT terminal connections on the PM820 and PM850 meters.
Resolution:
The terminal screws are 6-32 standard screws. Each meter is supplied with spade lugs that accommodate 14-16 AWG wire.
A user requires the information of the screw size and wire size, for the CT and PT terminal connections on the PM820 and PM850 meters.
Product Line:
PM800 series meters
Cause:
A user requires the information of the screw size and wire size, for the CT and PT terminal connections on the PM820 and PM850 meters.
Resolution:
The terminal screws are 6-32 standard screws. Each meter is supplied with spade lugs that accommodate 14-16 AWG wire.
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: