搜尋常見問題
Can “XML Import Module” in the VIP read CDATA (Character Data) elements from an XML page?
CDATA elements within XML files are just long strings of characters, not actual XML data. (CDATA = Character Data). The XML Module in the VIP cannot read CDATA elements. In fact, it can only read numeric elements, like <guid> in the example.
To properly read the info that's in the CDATA section, it would have to be first transformed into actual XML elements, i.e. with an XSL stylesheet.
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: