{}
搜尋常見問題
Can you install OPC for ION Enterprise at a later point in time (i.e. not during initial installation)?

The files required for OPC support are installed during the initial installation even if the OPC option was not originally purchased. A new product key can be purchased at any time that will unlock this capability.
The new product key must be entered in the License Manager in Management Console which will allow the ION OPC Data Access service to start. It is not necessary to re-install ION Enterprise.




Original article#16499
Last Revised: October 31, 2007
Public
All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL189247 V1.0, Originally authored by KBAdPM on 11/16/2007, Last Edited by KBAdPM on 11/16/2007
Related ranges: ION Enterprise V5.6, ION Enterprise V5.5, ION Enterprise V5.0

施耐德電機Taiwan