搜尋常見問題
ION8600: How to energize a High Voltage PSU meter in the lab with a Single Phase.
In the High Voltage PSU unit, power supply is energized from the blades of the meter. Internally, the PSU is connected to V1 of the meter. Hence, in order to energize the meter, make sure V1 is supplied with 120V.
Date Created: February 20, 2009
Last Revised: April 29, 2009
Public
Original Author: KG
All content © 1992-2009 Schneider Electric
Legacy KB System (APS) Data: RESL198388 V1.0, Originally authored by MiNe on 04/29/2009, Last Edited by MiNe on 04/29/2009
Related ranges: ION8600
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: