Issue
1. If the meter is powered up with a dead battery or a disconnected/loose battery it will show a checkerboard pattern on the screen for several seconds.
2. All configurations applied to the meter such as PT/CT ratios, Integrator values and other framework changes will be lost.
Product Line
ION7330 ION7350
Environment
Meter Behavior
Cause
When the battery is dead or disengaged and it is power cycled, the meter performs a factory initialization. A factory initialization causes the meter to lose its configuration data and custom template changes.
Resolution:
This issue cannot be fixed in the field. If you experience this issue and are unable to utilize the workaround below, please contact Schneider Electric or distributor to initiate an RMA to return the meter to the factory for battery replacement while available.
Workaround
Ensure the meter is not power cycled. This can be accomplished via a backup power supply such as a UPS.
Note: This behavior does not apply to the 7300-meter types, but the resolution is the same.
*Please note: The batteries on the 7330/7350 meter are meant to last for at least 10 years. The battery life can be checked from the front panel under Name Plate info. Option. Unfortunately, the battery life percentage indicator is meaningless if the battery is already dead, and the meter has been power cycled.*
發佈於: 施耐德電機Taiwan


Yunzhibao Foodstuff, a leading Chinese confectionary producer and exporter, partnered with Schneider Electric to build a smart factory so it could meet changing market demands. By implementing a comprehensive automation and digital solution based on EcoStruxure, including industrial software, it improved production efficiency and quality control. With optimised production processes and an intelligent management system, Yunzhibao Foodstuff's new factory has become more adaptable, efficient, and stable.