搜尋常見問題
Timestamps Displayed in the Different Components of ION Enterprise and ION Devices
Goals and Symptoms
This article explains how ION Enterprise and ION devices display timestamps.
Facts and Changes
Real-time data
Historical data
Timestamp
WebReach
Vista
Reporter
Clock module
Causes and Fixes
All timestamps are stored in the database by ION Enterprise using UTC format. However, different settings are used to display real-time and historical data, which may confuse the user.
Vista
For real-time data, Vista displays the meter time in local time according to the time zone settings of the client's operating system. For historical data, Vista displays the timestamps as calculated using the server operating system's time zone settings (assuming the option Show Logs in Universal Time (UTC) is unchecked).
Reporter
Reporter, like Vista, applies the time zone offset settings on the local PC to the UTC time to get the Local Time column.
WebReach
For real-time data screens, WebReach displays the meter time in local time according to the meter (i.e. according to the time zone settings on the meter). For historical data, WebReach displays the timestamps as calculated using the server operating system's time zone settings.
ION Devices Front Panel
The time zone settings on the meter (in the Clock module) allow the meter to display the local time.
-
Original article#10767
Public
All content © 1992-2007 Schneider Electric
Legacy KB System (APS) Data: RESL188928 V1.0, Originally authored by KBAdPM on 11/07/2007, Last Edited by KBAdPM on 11/07/2007
Related ranges: ION Enterprise V5.5