Issue
After connecting a VAMP 10L (VAM10LSE) module to a VAMP 321 the error light is illuminated.
Product Line
VAMP 321
VAMP ARC Flash Modules
Cause
The VAMP module must be configured to talk to the VAMP 321. Until this communication connection is established the VAMP 10L module will be in an error status. (This is also for any other ARC Flash Module)
Resolution
Connect to the VAMP 321 using the VAMPset software. Navigate to the ARC Protection screen, then click on the Install arc sensors and I/O units > select install, then write the changes to the VAMP 321. The VAMP 321 will locate all I/O devices along with any connected sensors.
發佈於:施耐德電機Taiwan