搜尋常見問題
What is the state of the ATS48 Fault relay for various conditions?
Issue:
State of the ATS48 Fault relay contact for the following conditions
Product Line:
Altistart ATS48
Environment:
All models
Cause:
None
Resolution:
Relay R1 functions as a fault relay on terminals R1A-R1C when Menu IO, parameter r1 = r1F.
It is a normally open contact.
Conditions:
Control power not applied to CL1-CL2, contact is OPEN
Control power applied and no fault, contact is CLOSED
ATS48 detects a fault, contact is OPEN
Note special case where Automatic Restart is active, Menu PrO, parameter ArS = ON. When an Auto-Reset condition is detected, the R1 contact will remain CLOSED until all restart attempts are completed. If the fault remains after the last attempt, then the R1 contact will OPEN.
State of the ATS48 Fault relay contact for the following conditions
Product Line:
Altistart ATS48
Environment:
All models
Cause:
None
Resolution:
Relay R1 functions as a fault relay on terminals R1A-R1C when Menu IO, parameter r1 = r1F.
It is a normally open contact.
Conditions:
Control power not applied to CL1-CL2, contact is OPEN
Control power applied and no fault, contact is CLOSED
ATS48 detects a fault, contact is OPEN
Note special case where Automatic Restart is active, Menu PrO, parameter ArS = ON. When an Auto-Reset condition is detected, the R1 contact will remain CLOSED until all restart attempts are completed. If the fault remains after the last attempt, then the R1 contact will OPEN.
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: