Issue
What processor are used in the Preventa XPSMF35 Safety controller
What processor are used in the Preventa XPSMF35 Safety controller
Product Line
XPSMF35
Resolution
The XPSMF35 controllers are equipped with 2 microprocessors for the safety-related processing (CPU) and 1 microprocessor for the communications (COM).
The CPU and COM Processors are 32-bit processors.
CPU: Motorola Coldfire MCF 5206e
Clock Speed: 40 MHz / 36 MIPS (54 Mhz / 50 MIPS)
COM: Motorola Power PC 860
Clock Speed: 50 MHz / 66 MIPS (66 Mhz / 88 MIPS)
發佈於: 施耐德電機Taiwan