搜尋常見問題
When my Network Management Card loses power, which log file(s) will be saved?
Issue
When my Network Management Card (or device with an embedded Network Management Card) loses power, which log file(s) will be saved? Which log files are saved when I install the Network Management card into a new device (if possible)?
Product Line
- Network Management Card 1 (NMC1) - AP9617, AP9618, AP9619
Devices with an embedded Network Management Card 1 include (but are not limited to): Metered/Switched Rack PDUs (AP78XX, AP79XX), Rack Automatic Transfer Switches (AP77XX, Environmental Monitoring Units (AP9320, AP9340, Netbotz 200)
- Network Management Card 2 (NMC2) - AP9630/AP9630CH, AP9631/AP9631CH, AP9635/35CH
pre-2022 2G Metered/Switched Rack PDUs (AP86XX, AP88XX, AP89XX), Rack Automatic Transfer Switches (AP44XX), Certain Audio/Video Network Management Enabled products.
- Network Management Card 3 (NMC3) - AP9640, AP9641, AP9544
Devices with an embedded Network Management Card 3 include (but are not limited to): Metered/Switched Rack PDUs (AP84XX, AP86XX, AP88XX, AP89XX, APDU9), Rack Automatic Transfer Switches (AP44XXA), Smart-UPS Online (SRT).
Environment
- All serial numbers
- All firmware versions (unless otherwise specified)
- Scenarios where the UPS Network Management Card or embedded Network Management Card has lost power or is transferred to a new device.
Cause
This information is provided on an informational basis. It may also be helpful when the Network Management Card device is power cycled, replaced, or installed into a different device type. Lastly, this may also be helpful in debugging issues, especially with a UPS where the original UPS is unavailable or has experienced a potential failure and a user wishes to view the logs from the installed Network Management Card. Depending on the scenario, these logs may be available if the Network Management Card is installed into another UPS to power the Network Management Card.
Resolution
Typically, the data log being saved or lost after a particular action, such as a power loss or re-installation, depends on the device's Network Management Card application. If your application is not listed, please contact APC Technical Support for further assistance to help verify the expected behavior, if required, to know before performing an action with your device.
The Network Management Card event log (event.txt) and configuration file (config.ini) are always saved after a power loss. Depending on your device type, you may find that the data log is not. Please refer to the chart below for more information.
Network Management Card Type | Device Type | NMC Application Module Name | Device Communication Language | Data Log Remains Intact after NMC Power Loss and/or Re-installation (Y/N) |
NMC1 - AP9617/18/19 | Smart UPS - SU, SUA, SUM, SURT, SURTA model prefix | sumx | UPS-Link | Yes |
NMC1 - AP9617/18/19 | Smart UPS - SURTD model prefix | sumx | Micro-link | Yes |
NMC1 - AP9617/18/19 | Symmetra LX | sy | UPS-Link | Yes |
NMC1 - AP9617/18/19 | Symmetra Power Array (MiniFrame/MasterFrame/RM) | sy | UPS-Link | Yes |
NMC1 - AP9617/18/19 | Remove from UPS-Link UPS and re-install into Micro-Link UPS | sumx | UPS-Link->Micro-Link | No |
NMC1 - AP9617/18/19 | Remove from Micro-Link UPS and re-install into UPS-Link UPS | sumx | Micro-Link->UPS-Link | No |
NMC1 - mini embedded AP9617 | AP7XXX series Rack Power Distribution Unit (PDU) | rpdu | N/A | Yes |
NMC1 - mini embedded AP9617 | AP77XX series Rack Automatic Transfer Switch (ATS) | g2ats | N/A | Yes |
NMC2 - mini embedded AP9538 | AP44XX series Rack Automatic Transfer Switch (ATS) | ats4g | N/A | Yes |
NMC2 - AP9630/31 | Smart UPS - SU, SUA, SUM, SURT, SURTA model prefix | sumx | UPS-Link | Yes |
NMC2 - AP9630/31 | Smart UPS - SURTD model prefix | sumx | Micro-link | Yes |
NMC2 - AP9630/31 | Smart UPS - SMT/SMX model prefix | sumx | Micro-link | Yes |
NMC2 - AP9630/31 | Symmetra LX | sy | UPS-Link | Yes |
NMC2 - AP9630/31 | Symmetra Power Array (MiniFrame/MasterFrame/RM) | sy | UPS-Link | Yes |
NMC2 - AP9630/31 | Smart UPS RT 2G - SRT model prefix (available in 2014) | sumx | Micro-Link | Yes |
NMC2 - mini embedded AP9630 | AP8XXX series Rack Power Distribution Unit (PDU) | rpdu2g | N/A | Yes, after power cycle. For re-installation of display module, may depend on if re-installed to same PDU model type. |
NMC2 - AP9630/31 | Remove from UPS-Link UPS and re-install into Micro-Link UPS | sumx | UPS-Link->Micro-Link | No |
NMC2 - AP9630/31 | Remove from Micro-Link UPS and re-install into UPS-Link UPS | sumx | Micro-Link->UPS-Link | No |
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: