搜尋常見問題
How to program an ATV61/71 drive to show speed as percentage instead of frequency?
Issue:
Programming an ATV61/71 drive to show speed as percentage instead of frequency.
Product Line:
ATV61, ATV71
Environment:
All models and serial numbers
Cause:
None
Resolution:
Show Output Frequency As a Percentage- go to menu 2 , Access level = advanced or expert
- go to menu 7 , Display config menu
- go to menu 7.1, User parameters menu
- go to "Parameter selection"; choose Menu 1.2 [Monitoring].
- Select “Output Frequency”
- Esc until come back to the 7.1 User parameters menu
- Go to the "Customized selection "
- Select “Output Frequency”
- If you want to change the name from “Output Frequency to Output Percentage
- Choose “User Name”
- Turn the thumb wheel to scroll to the letter “O” then press the F3 button to move the cursor to the rightmost position, repeat selecting the next letter. (note: to move back press F2 and to end and save this custom name press enter)
- Select “Unit” and select “%”
- Select “Multiplier” and enter “10”
- Select “Divisor” and select “6”
- Press Esc back to the MAIN MENU
- Press enter on the DRIVE MENU.
- Scroll to the MONITORING menu and press enter
- Scroll to the customized “User Name” you entered above.
- You should see the output frequency shown as a percentage.
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: