Issue:
Notification fails to work when an event is triggered.
Product:
PowerChute Network Shutdown versions 3.1
Environment:
IBM AIX, HP-UX, Solaris
Cause:
Install PCNS 3.1 on IBM AIX/HP-UX/Solaris Server. Configure PCNS in single mode or any other configuration and navigate to Configure event page. Enable notification for any event. Trigger the event for which notification is enabled.
Expected Result: Notification should be received
Actual Result: Notification is not received
Resolution:
Upgrade to PowerChute Network Shutdown version 4.x
發佈於:施耐德電機Taiwan