搜尋常見問題
Is there a roof fan available for the NetShelter SV cabinets?
Issue:
There does not appear to be an optional roof fan for the NetShelter SV cabinets.
Product Line:
NetShelter SV
Environment:
All versions and serial ranges.
Cause:
A request has been made to add a roof fan to a NetShelter SV.
Resolution:
The NetShelter SV cabinets do not currently have roof fans available.
Some of the fans that can be used inside the SV cabinet are: ACF001, ACF002, ACF003, ACAC40001, ACF201BLK, ACF202BLK.
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: