{}
搜尋常見問題
Are the ATV12 drives CE approved?
Issue:
ATV12 drives CE approved.

Product Line:
ATV12

Environment:
All ATV12 drives

Cause:
Are the ATV12 drives CE approved?

Resolution:
Yes they are CE approved. Can see this listed on the ATV12 Characteristics (page 2 of document  60401-EM-indd).

施耐德電機Taiwan

探索更多
系列:
可能有幫助的文章
探索更多
系列: