{}
搜尋常見問題
Can I hot swap a CPS1xx xx Power Supply?
Issue:

No, the 140CPS110 00 cannot be hot swapped when supporting a CPU. Doing so will interrupt the CPS hold up time which the CPU will need in order to back up the program.


Product Line: Quantum


Environment:n/a


Cause:n/a


Resolution:n/a


R-101317

施耐德電機Taiwan

探索更多
系列:
可能有幫助的文章
探索更多
系列: