搜尋常見問題
What is the minimum and maximum LexCom Delta 8) cable?
Legacy -
The minimum and maximum single length that can be run is minimum of 2 metres and a maximum of 50 metres. Cables are installed in a star configuration and should be segregated form any mains cabling.
The minimum and maximum single length that can be run is minimum of 2 metres and a maximum of 50 metres. Cables are installed in a star configuration and should be segregated form any mains cabling.
A bend radius of 25mm is recommended
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: