搜尋常見問題
What is the difference between a removable locking device and a fixed locking device for the Compact NS and NSX 100 to 630 range.
The removable locking device enables the MCCB to be locked in the OFF position only and is removable from the device.
![29370 Removable Lock device](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H0000088ZEWQA2&oid=00DA0000000abSm)
The fixed locking device enables the MCCB to be locked in the OFF or ON position but is fixed to the device.
The fixed locking device enables the MCCB to be locked in the OFF or ON position but is fixed to the device.
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: