{}
搜尋常見問題
Prima P / what is the spacing rods 04691 kit composition / dimensions
The 04691 kit is composed of Insulated threaded parts made of Epoxy glass:
1 rod M10, length 475mm + 2 square nuts (thickness 10mm for a 17mm tool)
Also included: 3 thermoplastic tubes diameters int./ext: 12mm/30mm - length 60mm.
And 2 metallic washers (thickness1.6mm)

施耐德電機Taiwan