搜尋常見問題
What is the MTBF on the BMXNRP0200?
Issue:
What is the MTBF on the BMXNRP0200?
Product Line:
BMXNRP0200
Resolution:
What is the MTBF on the BMXNRP0200?
Product Line:
BMXNRP0200
Resolution:
Product | Mtbf 30° Continuous | Mtbf 30° Intermittent | Mtbf 60° Continuous | Mtbf 60° Intermittent | Mtbf 85° Continuous | Mtbf 85° Intermittent | Nb Cpt Missing | Nb Cpt Missing * Qty | Nb Cpt Total * Qty | Ratio Nb Cpt Missing / Nb Cpt Total |
BMXNRP0200 | 2118895.462 | 1579125.228 | 1394785.733 | 1135803.479 | 890993.217 | 779988.004 | 7 | 13 | 381 | 3.40% |
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: