搜尋常見問題
When did the ATV18 drive become obsolete?
Issue: Is the ATV18 become obsolete? Product line: ATV18, Altivar 18 Environment: All models, all serial numbers Cause: Determine age of unit, product obsolescence Resolution: ATV18 became obsolete in 1995. The current replacement is the ATV12, ATV312 or ATV320 depending on the application (Current, HP and Voltage of the motor). There are some differences in dimensions, wiring and programming that should be reviewed by the customer. |
發佈於:施耐德電機Taiwan
探索更多
產品:
探索更多
產品: