搜尋常見問題
What's the limitation of M258 expansion modules and I/O number.
1) Modules Max: The bus allows to add local IO and remote IO up to 250 slices IO.
2) Typical total TM5 digital I/O needs: Up to 2400 I/Os (Including Local & Remote racks)
3) M258 logic controller enables up to 200 analog I/Os and/or temperature modules to be connected
4) Maximum number of %IW/%QW: 4096 bytes for the Input and 4096 bytes for the Output.
2) Typical total TM5 digital I/O needs: Up to 2400 I/Os (Including Local & Remote racks)
3) M258 logic controller enables up to 200 analog I/Os and/or temperature modules to be connected
4) Maximum number of %IW/%QW: 4096 bytes for the Input and 4096 bytes for the Output.
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: