搜尋常見問題
Pin-out for VX003 PC cable for RS232 port of VAMP 200 series
Issue:
Trying to connect to the VAMP 200 series through the RS232 port fails.
Product Line:
VAMP 255, VAMP 257, VAMP 259, VAMP 200 series, VX003
Environment:
Connecting to VAMP set to configure settings.
Cause:
The RS232 port configuration is not a standard RS232 port.
Resolution:
![Image 1 Image 1](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000008zpIhQAI&oid=00DA0000000abSm)
Trying to connect to the VAMP 200 series through the RS232 port fails.
Product Line:
VAMP 255, VAMP 257, VAMP 259, VAMP 200 series, VX003
Environment:
Connecting to VAMP set to configure settings.
Cause:
The RS232 port configuration is not a standard RS232 port.
Resolution:
發佈於:施耐德電機Taiwan
探索更多
產品:
系列:
探索更多
產品:
系列: