搜尋常見問題
Video: How do you put the ATV12 drive in local mode to run off the face of the drive?
Issue:
Turn an ATV12 drive in local mode to run
Product Line:
Altivar ATV12
Environment:
All
Cause:
Requirement to operate the ATV12 in local mode using the wheel for speed control and the start stop buttons for starting and stopping.
Resolution:
Programming:
Turn an ATV12 drive in local mode to run
Product Line:
Altivar ATV12
Environment:
All
Cause:
Requirement to operate the ATV12 in local mode using the wheel for speed control and the start stop buttons for starting and stopping.
Resolution:
Programming:
- Hold the MOD button for 3 to 4 seconds to put this drive in local mode.
- You will see LOC displayed followed by rdY.
- While in Local Mode, 3 LEDs will flash top to bottom on the left side of the display to indicate Local Mode is activated.
- If you need to go back to remote mode hold the MOD button again for 3 to 5 seconds.
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: