{}

我們的品牌

Impact-Company-Logo-English Black-01-177x54

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
搜尋常見問題
What are the conditions for closing the ATS48 R2 relay?
Issue:
ATS48 R2 relay closing conditions

Product Line:
Altistart 48

Environment:
All models

Cause:
None

Resolution:
The R2 relay is an End of Starting relay. It has a dedicated function to control a shorting contactor. It is not programmable.
The relay contact is normally open and will close when the motor is up to full speed.
The conditions for R2 closure are:
- If CLP = OFF, relay closes when the thyristors are full wave (angle = 1), full voltage is being sent to the motor.
- If CLP = ON, relay closes when the thyristors are full wave (angle = 1) and the peak current estimated is less than 1.4 x In.

施耐德電機Taiwan

探索更多
系列:
可能有幫助的文章
探索更多
系列: