搜尋常見問題
Can I save and transfer parameters from an ATV312 drive to another using the VW3A1101 external keypad?
Issue:
Can VW3A1101 external keypad save and transfer parameters between two ATV312 drives?
Product Line:
ATV312
Environment:
All serial numbers for ATV312
Cause:
N/A
Resolution:
No, this drive and keypad do not support that feature.
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: