Issue:
ATV312 Safe Torque Configuration
Product Line:
ATV312
Environment:
All serial numbers for ATV312
Cause:
N/A
Resolution:
No, the ATV312 does not have a Safe Torque Off option. That feature is only compatible with the ATV32, ATV320, ATV61, ATV71 , ATV630 and ATV940 drives
ATV312 Safe Torque Configuration
Product Line:
ATV312
Environment:
All serial numbers for ATV312
Cause:
N/A
Resolution:
No, the ATV312 does not have a Safe Torque Off option. That feature is only compatible with the ATV32, ATV320, ATV61, ATV71 , ATV630 and ATV940 drives
發佈於:施耐德電機Taiwan