The criterias that effects the cost when changing the IP rating of the enclosure ona TRIHAL cast resin dry type transformer is rated power, insulation level and losses.
我願意透過電子通訊方式(如電子郵件)從施耐德電機及其附屬公司接收新聞和商業資訊,我也同意他們收集這些電子郵件的開啟和點擊資訊(使用隱藏式追蹤像素),以衡量溝通效益並優化這些資訊。如您需更多詳細資訊,請參閱施耐德電機的 隱私權政策