{}

我們的品牌

Impact-Company-Logo-English Black-01-177x54

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
搜尋常見問題
Where to reconfigure, in BLAT, the SMTP server parameter
Issue
BLAT is configured on server to send out email using the Launching Module in VIP. The SMTP server has changed and need to reconfigure in BLAT.

Product Line
SPM7.x
PME7.x
Power Monitoring Expert (PME 8.x)

Environment
Windows

Cause
BLAT is configured on server to send out emails using the Launching Module in VIP. The SMTP server has changed and need to reconfigure BLAT

Resolution
When BLAT was configured on the server the install command only stores the various parameters in the Windows Registry. To change or verify the SMTP settings navigate to Regedit ->HKEY_LOCAL_MACHINE ->SOFTWARE ->Wow6432Node ->Public Domain ->Blat. The configured parameters that BLAT uses can be found here.

施耐德電機Taiwan

探索更多
產品:
可能有幫助的文章
探索更多
產品: