搜尋常見問題
Can you use the Lonworks card from an ATV21 on an ATV212 and vice versa?
Issue:
Usage of a Lonworks card from an ATV21 on an ATV212 and vice versa
Product Line:
Altivar 21, Altivar 212
Environment:
All
Cause:
N/A
Resolution:
No.
The ATV21 drive's lonworks card part number is VW3A21312.
The ATV212 drive's lonworks card part number is VW3A21212.
Usage of a Lonworks card from an ATV21 on an ATV212 and vice versa
Product Line:
Altivar 21, Altivar 212
Environment:
All
Cause:
N/A
Resolution:
No.
The ATV21 drive's lonworks card part number is VW3A21312.
The ATV212 drive's lonworks card part number is VW3A21212.
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: