我們的品牌

Impact-Company-Logo-English Black-01-177x54

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Could TSXCBY380KT transmit data over 1Mbyte per second
Background:
Customer is using  TSXCBY380KT for a project which requires large amounts of data transmission
The datesheet of TSXCBY380KT has no announcement of transmission capacity.

Question:
Could TSXCBY380KT transmit data over 1Mbyte per second?

Answer:
Yes, it could transmit data over 1Mbyte per second from cable SPEC