{}
搜尋常見問題
How to set up an ATV12 drive to run up to 60Hz?
Issue:
ATV12 set-up to run up to 60Hz

Product Line:
Altivar 12

Environment:
All Serial number

Cause:
N/A

Resolution:
Go into CONF menu.
Set BFR to 60 Hz.
Make sure HSP is set to 60 hz.

施耐德電機Taiwan

探索更多
系列:
可能有幫助的文章
探索更多
系列: