搜尋常見問題
I want to upgrade a BMXCRA31200 or BMXCRA31210 or BMECRA31210, that is not yet configured. How shall I proceed.
- Set the rotary switches of the CRA to "stored"
- Power cycle the CRA
- Plug the PC with UnityLoader on the CRA's service port
- Use the 10.10.mac5.mac6 @ on UnityLoader
- Transfer the firmware.
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: