搜尋常見問題
Video: Why won't the ATV630 drive run in reverse?
Issue:
ATV630 won't operate in reverse.
Product line:
ATV600, ATV630, ATV650, Altivar Process
Environment:
All
Cause:
Configuring Reverse Motor Operation on Altivar 630 Process Drives
Resolution:
The Factory settings for the Process Drive to run in reverse is not allowed.
To allow Reverse operations:
Go to Complete Settings > Command and Reference > Reverse Disable, change the setting from Yes (meaning Reverse is not allowed) to No (meaning Reverse is allowed) and save. Now, you should be able to operate the drive in Reverse.
ATV630 won't operate in reverse.
Product line:
ATV600, ATV630, ATV650, Altivar Process
Environment:
All
Cause:
Configuring Reverse Motor Operation on Altivar 630 Process Drives
Resolution:
The Factory settings for the Process Drive to run in reverse is not allowed.
To allow Reverse operations:
Go to Complete Settings > Command and Reference > Reverse Disable, change the setting from Yes (meaning Reverse is not allowed) to No (meaning Reverse is allowed) and save. Now, you should be able to operate the drive in Reverse.
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: