搜尋常見問題
What are errors E1300 and E1301 on the LXM32 drive?
Issue:
Errors E1300 and E1301 on the LXM32 drive
Product Line:
LXM32
Resolution:
E1300 means a safety STO function is activated (STO_A, STO_B)
E1301 means the levels of the inputs STO_A and STO_B were different for more than 1 second
These 2 errors are related to a bad wiring of inputs STO_A and STO_B, a bad 24V power supply or an activated emergency stop, which cuts the 24VDC from the STO inputs.
Making sure the STO inputs are getting 24VDC before powering the drive will reset these faults.
Errors E1300 and E1301 on the LXM32 drive
Product Line:
LXM32
Resolution:
E1300 means a safety STO function is activated (STO_A, STO_B)
E1301 means the levels of the inputs STO_A and STO_B were different for more than 1 second
These 2 errors are related to a bad wiring of inputs STO_A and STO_B, a bad 24V power supply or an activated emergency stop, which cuts the 24VDC from the STO inputs.
Making sure the STO inputs are getting 24VDC before powering the drive will reset these faults.
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: